Conext Configuration Tool
This product is discontinued for the Australia market. For technical support, please visit here.
Part number: 865-1155-01
This product is discontinued for the Australia market. For technical support, please visit here.
Part number: 865-1155-01
The Conext™ Configuration tool is a PC-based software used by system installers to calibrate multi-unit systems during system configuration and reduce installation time. The Conext Configuration tool is not meant to replace the Insight or any other monitoring devices. Those monitoring devices may still be required to monitor Schneider Electric solar and storage system and components. Software and drivers for the Conext Configuration Tool are under the downloads section (Firmware). Conext Config USB Driver is firmware used for general installation setup. Conext Config Tool Software_AI (Anti-Islanding) is used when 2 or more inverters are installed in parallel on a single phase connection (See Conext XW+ Multi-Unit Power System Design Guide under the downloads section (Technical Publications). It is also used if there is a specific requirement by a utility.
Note: Adjustment of AC anti-islanding parameters should only be done after consultation with the power utility or authority having jurisdiction.