InsightHome and InsightFacility Edge Devices
Easily connects with Insight software for simplified energy management of solar and storage systems.
Secure power for your home during grid outages by retrofitting your grid-tied system with backup power using proven Schneider Electric’s solutions.
During grid outages PV Inverter production cannot occur, so a home with a PV inverter system installed will not have power during an outage. However for homes that have a PV Inverter system installed and are already selling power to the grid, it is still possible to retrofit backup power using the XW Pro or SW inverter chargers. In a FIT program either XW Pro or SW is added behind PV inverter to provide backup, no change to PV inverter FIT wiring is required. However backup power is limited to the capacity of the battery bank and the solar system cannot be used to charge the batteries while the grid is down. In a NET metered program the XW Pro inverter charger is added in front of PV inverter to provide backup power. The PV inverter is rewired from the grid connection to critical load subpanel and AC Couple is on AC Output port. Our solutions indlue:
Easily connects with Insight software for simplified energy management of solar and storage systems.
Battery bank monitoring that can detect battery string imbalances before performance is impacted.
Designed for reliability, the AGS automatically starts or stops a generator to meet your power needs.
The perfect hybrid inverter solution for off-grid, backup power, and self-consumption needs.
The XW Conduit Box provides a clean, professional finish that safely protects end-users from contact with wiring
Powerful, yet simple energy management software that provides users with access to critical system information.
Protect your home’s power supply from grid outages and save on energy costs with utility time of use and demand charge optimization.