InsightHome and InsightFacility Edge Devices
Easily connects with Insight software for simplified energy management of solar and storage systems.
Reduce your electric bill and dependence on the electric utility company by going with a green power solution from Schneider Electric.
Enabled by PriorityPower the XW Pro and SW will prioritize the self-consumption of stored battery and PV generated power over grid power, helping homeowners avoid high utility charges. Both XW series and SW also provide for backup in areas prone to grid outages. Conext™ XW Pro and XW+ takes it one step further by enabling excess PV power to be sold using GridSell.
Coupling the PV system to the battery bank with Conext™ MPPT Solar Charge Controllers is the most efficient and economical method for self-consumption and for storing PV power. Both Conext™ XW series and SW will also charge the battery bank from the grid if solar irradiation is insufficient. Batteries and Solar PV can be scaled up as needed.
There are two main applications of ParallelPower:
Peak Load Shaving: The Conext™ XW Pro, XW+ and SW can limit the power draw from the utility connection by adding power above a set point to support large temporary loads, helping avoid peak usage charges in areas with the tier-based tariff on the capacity of incoming feed or on peak consumption.
Grid Boosting: The Conext™ XW Pro, XW+ and SW can supplement grid input with extra AC power to support large loads, temporarily boosting power within a home beyond the limit of the grid connection.
Conext™ solutions includes:
Easily connects with Insight software for simplified energy management of solar and storage systems.
Battery bank monitoring that can detect battery string imbalances before performance is impacted.
The perfect hybrid inverter solution for off-grid, backup power, and self-consumption needs.
Features flexible integration and MPPT multi-stage charging, supporting and improving battery life.
Install for less, and harvest more energy with the Conext MPPT 80 600.
Offers optimum system performance with flexible installation of DC Coupled solar and storage systems.
The XW Conduit Box provides a clean, professional finish that safely protects end-users from contact with wiring
Powerful, yet simple energy management software that provides users with access to critical system information.
Protect your home’s power supply from grid outages and save on energy costs with utility time of use and demand charge optimization.