InsightHome and InsightFacility Edge Devices
Easily connects with Insight software for simplified energy management of solar and storage systems.
As electricity prices increase, maximize your total savings on energy costs with our hybrid solution for small commercial enterprises.
Enabled by PriorityPower Conext™ XW+ will prioritize the self-consumption of stored battery and PV generated power before purchasing grid power, helping business owners avoid high utility charges. XW+ will also provide for backup in areas prone to grid outages. Conext™ XW+ takes it one step further by enabling excess PV power to be sold using GridSell
Coupling the PV system to the battery bank with Conext™ MPPT Solar Charge Controllers is the most efficient and economical method for self-consumption and for storing PV power. Both Conext™ XW+ and SW will also charge the battery bank from the grid if solar irradiation is insufficient. Batteries and Solar PV can be scaled up as needed. There are two main applications for ParallelPower:
Grid Boosting: Conext™ XW+ and SW can supplement the grid input with the extra power to support large loads, temporarily boosting power within a building with limited grid supply.
Peak Load Shaving: Conext™ XW+ can limit the power draw from the utility connection by adding power above a set point to support large temporary loads, helping avoid peak usage charges.
Conext™ solutions include:
Prioritize consumption of solar power with PriorityPower
Avoid utility demand charges with ParallelPower
Temporarily increase power within the home with ParallelPower
Take advantage of the lower lifetime cost of Lithium-Ion batteries with ChargePower technology
Sell power to the utility with GridSell (Conext™ XW+)
Easily connects with Insight software for simplified energy management of solar and storage systems.
Scalable and flexible, the CL 30/50 is the ideal solar solution for commercial buildings.
Battery bank monitoring that can detect battery string imbalances before performance is impacted.
Features flexible integration and MPPT multi-stage charging, supporting and improving battery life.
Install for less, and harvest more energy with the Conext MPPT 80 600.
Offers optimum system performance with flexible installation of DC Coupled solar and storage systems.
The XW Conduit Box provides a clean, professional finish that safely protects end-users from contact with wiring
Powerful, yet simple energy management software that provides users with access to critical system information.
Protect your home’s power supply from grid outages and save on energy costs with utility time of use and demand charge optimization.