This product is discontinued. For technical support, please visit here.

The local and remote interface to the Conext SmartGen™ Power System.

Conext™ Viewer is a user-friendly application for accessing the Conext SmartGen™ Power System. It is used to monitor and configure the Conext SmartGen™ Power System, and it also provides advanced features for troubleshooting. Users logon to Conext™ Viewer using their unique credentials and access the Conext SmartGen™ Power System using either via a wired or wireless connection. Remote connection to the Conext SmartGen™ Power System is also supported by Conext™ Viewer.