This product is discontinued. For technical support, please visit here.

Containerized plug and play power conversion system adapted to customer requirements and local standards

The PV Box ST is a power conversion system. In a PV plant installation, it operates between DC field and AC MV grid connection point. The PV Box performs the DC power concentration, the DC/AC conversion and the AC voltage elevation to the grid voltage level. It ensures the protection of the maintenance people and the installation against electrical faults such as short-circuit and lightning. The optimized versions of the PV Box allow a reduction of the balance of systems cost, an increase of the reliability and an improvement of construction lead times.