Whole home or partial home backup made easy. For USA and Puerto Rico.

When paired with Schneider Electric XW Pro inverters, the Backup Control Switch (BCS) automatically disconnects from the grid during an outage, allowing the system to provide backup power to the home.

Certified to UL standards for USA, the Backup Control Switch is used for larger XW Pro systems requiring up to 200 A rated MID or service entrance installation.

Part number: 865-BCS-2200