Discontinued Product
Conext XW (120) Solar Inverter System
Conext™ XW is an adaptable pure sine wave, single-phase, split-phase or three-phase inverter/charger system with global grid-tie functionality and dual AC power inputs. Available solar charge controllers, monitoring, and automated generator control modules enable further adaptability. From single Conext XW unit to multiple clusters of units, up to 36 kW each, the Conext XW is a scalable system that allows for the integration of solar capacity as required. Adaptable and scalable, the Schneider Electric Conext XW system is the one solution for global grid-interactive and off-grid, residential and commercial, solar and backup power applications.
*For the latest generation of the Conext XW hybrid inverter please visit Conext XW Pro page.